Johannesburg, February 15, 2012
Siemens Hearing Solutions and the University of the Witwatersrand’s Department of Speech Pathology and Audiology joined forces to test the hearing of 500 learners at Isekelo Primary School.
The tests were conducted over two days, the 9th and 10th of February, during which time learners in grades R 1 and 2 underwent a series of tests including an otoscopic exam (a physical test of the ear canal and tympanic membrane); tympanometry to test the functionality of the middle ear; and audiometric screening, to assess hearing levels. Michelle Reyneke, CEO of Siemens Hearing Solutions, explains that these three tests make up a basic test battery, and make it possible to identify possible hearing problems or obstructions within the ear. “In cases where such issues were identified, the children were referred for further diagnostic testing,” she says.
Also participating in the drive are audiologists from the University of the Witwatersrand Department of Speech Pathology and Audiology, says Dr Karin Joubert, a lecturer at the department. They conducted the diagnostic testing on site.
“Approximately six to nine children out of every 1 000 individuals are born with or acquire hearing loss as a result of diseases like otitis media (ear infection) and meningitis,” Joubert says, pointing to the importance of hearing tests. Reyneke agrees, noting that although hearing tests are available from birth for those covered by private healthcare, the reality for many South Africans is that they are not able to access such tests, even at school. And yet it is imperative that any hearing problems be identified at this point, because they have the potential to impact significantly both on the child’s social interactions and on academic performance. “Sadly, often these problems are picked up only once it has become clear that a child’s performance at school is not up to standard. It’s critical, for the healthy development of the child, that they are identified as soon as possible,” Reyneke says.
Fortunately, if hearing problems are identified, intervention is possible, Joubert says. Indeed, as part of the initiative, Siemens Hearing Solutions sponsored a number of hearing instruments. The company also covered the cost of transport and meals for the children who had the testing done. Reyneke explains that Siemens Hearing Solutions is enthusiastic about playing an active role in its community and proud to contribute to the Isekelo Primary School during, a school Siemens adopted as part of its partner school programme.
“Our partnership with Wits is mutually beneficial: not only does the initiative provide students with useful exposure, but also because the clinical scope of the work means that the hearing tests are conducted with the utmost professionalism.” Meanwhile, Joubert says that service learning, of which community engagement is a critical component, is a key priority for the university. The University of the Witwatersrand has a proud tradition of taking part in such initiatives, making it an ideal partner for Siemens.
“The initiative was a great success and we hope that it will be the first of many,” Reyneke concludes.